Technical FAQs

Ask a Question

Can a PQ3610G plug-in unit be used instead of a PQ3210G? Will they both plug onto the same busway?

These two units would plug onto the same bus, but the PQ3610G requires 600V fuses, the PQ3210G requires 240V fuses. The units are exactly the same except for the fuse spacing.


CTA-ID : 2031755
Was this helpful?
What can we do to improve the information ?