Technical FAQs

Ask a Question

What are the differences between the SU3040D400CB and SU3040D400FB Combination Service Entrance Device All-in-Ones?

The SU3040D400CB is a surface mount device, convertible to semi-flush with a field installed FK400 flange kit (ordered separately). The SU3040D400FB is electrically equivalent, but is a semi-flush mount device only, with the semi-flush top endwall factory installed and sidewall flanges factory included.


CTA-ID : 2031649
Was this helpful?
What can we do to improve the information ?