Technical FAQs

Ask a Question

Will FA breakers accept two wires per phase?<br /><br />

No, generally, FA breakers can accept only one wire per phase. Power distribution connectors can be applied on LOAD side only of FAL breakers (but not I-Line circuit breakers), and it can accommodate multiple wires. Power distribution connectors are designed for UL508 Industrial control application and for UL19951995/CSA C22.2 No. 236 heating and cooling equipment. Available lugs are in Circuit Breaker section of Digest.

CTA-ID : 2031505
Was this helpful?
What can we do to improve the information ?