Technical FAQs

Ask a Question

Is there a relay that will close when the Altivar ATV66 unit is running?

The R2 relay can be programmed as running state and will energize when a run command is present, dc injection is not enabled, and there is not a fault on the drive controller. This relay has a NO and a NC contact.


CTA-ID : 7023
Was this helpful?
What can we do to improve the information ?