Technical FAQs

Ask a Question

How is the LDB Wireway cover held down?

The standard LDB wireway is hinged on one side and held down on the other side by screws. The exception is that 12`` x 12`` LDB is available in screwcover only.

CTA-ID : 2031583
Was this helpful?
What can we do to improve the information ?