Technical FAQs

Ask a Question

What transformers will the 2005 Energy Act impact?

It impacts all ventilated General Purpose transformers, including Watchdog and k Factor Rated Transformers. kVA ranges are 15 through 1000 kVA for Three Phase and 15 and 333 kVA Single Phase. It does NOTinclude the Drive Isolation Transformers, Resin Encapulated , Non-Ventilated, 9070 Control Transformers.


CTA-ID : 2031482
Was this helpful?
What can we do to improve the information ?