Technical FAQs

Ask a Question

Is there a lug for 800A Powerpact MGL and MJL breaker that will accept parallel 750 aluminum conductors?

The compression lug kit YA800P7 will accept (2) 750 kcmil conductors. There is no mechanical lug for Powerpact M-frame that will accept two 750 kcmil conductors.

CTA-ID : 2031449
Was this helpful?
What can we do to improve the information ?