Technical FAQs

Ask a Question

What coil codes are available for the U-Line motor starter Control Units?

The coil codes available for the U-Line Motor Starter control units are as follows:
24VDC is BL
24VAC is B
48-72V DC or 48V AC is ES
110-240V AC/DC is FU.
We do not have 480VAC coils available


CTA-ID : 2031577
Was this helpful?
What can we do to improve the information ?