Technical FAQs

Ask a Question

How is the Altivar ATV66 drive programmed to go to a preset speed if the speed reference follower signal is lost to AI2 analog input?

In Menu 7.4 Fault Management select Loss of Follower, then select Go to: ####Hz, enter the preset speed then press enter. If the speed reference drops to less than 3mA the drive will run at the preset speed.


CTA-ID : 7012
Was this helpful?
What can we do to improve the information ?