Technical FAQs

Ask a Question

What is the contact rating of an RM4 relay?<br /><br />

These are rated IEC - AC15, DC13; NEMA/UL B300 and have an 8 amp continuous current rating per page 3 of 8430CT0001.


CTA-ID : 2031647
Was this helpful?
What can we do to improve the information ?