Technical FAQs

Ask a Question

Is the DTU326 or DTU326R suitable for use as service equipment?

Issue:
Application

Product Line:
Double Throw Safety Switch

Cause:
Application

Resolution:
Yes, these switches are marked "suitable for use as service equipment". A neutral assembly is NOT provided as a standard feature. If a neutral assembly kit is required, order DT600NKD and bond the neutral to the enclosure with the bonding strap assembly provided with the neutral kit. 


CTA-ID : 2031606
Was this helpful?
What can we do to improve the information ?