Technical FAQs

Ask a Question

What is ``Control speed + error`` Fault on the Altivar ATV66?

It detects when the motor shaft is spinning faster than what the drive is calling. This fault detection can be disabled in Fault Management Menu 7.4.


CTA-ID : 7007
Was this helpful?
What can we do to improve the information ?