Technical FAQs

Ask a Question

Are ATV31 drives available in enclosures?

The ATV31 drives are primarily designed to be mounted in control panels.
There are conduit kits that can be added to the drives to allow them to meet type 1 enclosure requirements.
Please see the installation guide for mounting and temperature requirements.

Reviewed 8/2011


CTA-ID : 2031180
Was this helpful?
What can we do to improve the information ?