Technical FAQs

Ask a Question

Is there Ground fault detection on the Altivar ATV66?

Yes, ground fault detection is accomplished by monitoring current on the DC bus with a CT.


CTA-ID : 6988
Was this helpful?
What can we do to improve the information ?