Technical FAQs

Ask a Question

Where do the control wires go when I wire to the shunt trip accessory on a PowerPact H & Powerpact J frame I-Line mount breaker? There is a cover on the front of the breaker that has no holes in it.

The wires can be routed under the side of the front accessory cover and down the side of the breaker per the instruction bulletin that comes with the breaker.

CTA-ID : 2031574
Was this helpful?
What can we do to improve the information ?