Technical FAQs

Ask a Question

What is the fault relay contact status of the Altivar ATV66 when powered up and running?

The relay is energized and the contacts change state when the unit powers up and there are not any faults. If a fault occurs or line power is removed the contacts will revert to their normal unenergized state.

CTA-ID : 6998
Was this helpful?
What can we do to improve the information ?