Technical FAQs

Ask a Question

What is the temperature rating of the lugs on an NQOD-MLO panelboard?<br /><br />

They are rated for 75 degree C wire.





CTA-ID : 2031727
Was this helpful?
What can we do to improve the information ?