Technical FAQs

Ask a Question

What is the DIP switch AI2 - V or AI2 - I used for on the Altivar ATV66 drive control basket?

It switches the AI2 analog input to be either a 0-5VDC input when set to the AI2-V selection or a 4-20ma analog input when in AI-I position.

CTA-ID : 7019
Was this helpful?
What can we do to improve the information ?