Technical FAQs

Ask a Question

What is the word and bit for fault reset using serial communications with the ATV58?

Word 400 bit 7 resets faults when put into state of 1.
It is important to return this bit status back to 0 when the reset is complete.


CTA-ID : 2016003
Was this helpful?
What can we do to improve the information ?