Technical FAQs

Ask a Question

Is the output voltage that can be displayed with the Altivar ATV66 keypad a RMS value?

It is a RMS value.


CTA-ID : 7063
Was this helpful?
What can we do to improve the information ?