Technical FAQs

Ask a Question

What connections are available for the LA and LH type mission critical breakers, those with an MC suffix?

The LA-MC and LH-MC breakers have the same connection options as the standard LA and LH type breakers. This includes I-Line, lugs on one or both ends, and bus connected.


CTA-ID : 2031798
Was this helpful?
What can we do to improve the information ?