Technical FAQs

Ask a Question

Can a QO2DTI be used to reatain the 150a, 175a or 200a QO Branch Circuit Breakers to the Interior, when they are being Back-Fed in a Load Center?

No! The retaining kit that should be used when back-feeding a 150a, 175A or 200A branch circuit breaker in a QO Load Center, is a PK5RK.

CTA-ID : 2031486
Was this helpful?
What can we do to improve the information ?