Technical FAQs

Ask a Question

What are the differences between the CU816D400CB and CU816D400FB Combination Service Entrance Device Meter-Main?

The CU816D400CB is a surface mount device, convertible to semi-flush with a field installed FK400 flange kit (ordered separately). The CU816D400FB is electrically equivalent, but is a semi-flush mount device only, with the semi-flush top endwall factory installed and sidewall flanges factory included.

CTA-ID : 2031657
Was this helpful?
What can we do to improve the information ?