Technical FAQs

Ask a Question

How do HVL/cc and Motorpact sections lineup?

Issue:
Product Feature

Product Line:
INMVE - MV EQUIPMENT

Environment:
NEMA ICS 3, UL347, EEMAC G14-1, ANSI C19.7, IEC 60470, IEC 60529, IEC60694, IEC60129, IEC62271-102, IEC 62271-200, ANSI C37.20.7

Cause:
The physical arrangement and orientation of disparate equipment in a lineup must be known in order to successfully plan for its installation.

Resolution:
HVL/cc and Motorpact align in both front and rear.


CTA-ID : 2031487
Was this helpful?
What can we do to improve the information ?