Technical FAQs

Ask a Question

What is the coil burden of the LUB12 at 24vdc with the standard control modules?<br /><br />

It is 130mA inrush, 60mA sealed.


CTA-ID : 2032355
Was this helpful?
What can we do to improve the information ?