Technical FAQs

Ask a Question

What is the purposed of the motor cutoff switch?

The motor cutouff switch can be padlocked. This switch disables the motor circuit to keep the springs from recharging or the switch from being remotely operated by the motor.

Revised on 01/22/07

CTA-ID : 2032350
Was this helpful?
What can we do to improve the information ?