Technical FAQs

Ask a Question

On a 225a NQOD MLO panel, that is the torque value for the wire binding connector?<br />

Up to 2/0 cable use 180 inch pounds
300mcm cable use 250 inch pounds



CTA-ID : 2032347
Was this helpful?
What can we do to improve the information ?