Technical FAQs

Ask a Question

Customer has p/n 9037EG8R1F1. What is R1F1?

The 9037EG8 is manufactured without a rod or float. The customer can specify the float and rod part numbers for the components that he desires. These could be 9049ER1 and 9049EF1. To receive all components packaged in a single carton specify the float switch class 9049EG8 plus ``R`` and rod number and ``F`` and float number. Example: ``9037EG8R1F1. `` See p. 36 of 9034CT9701 Catalog.


CTA-ID : 2032346
Was this helpful?
What can we do to improve the information ?