Technical FAQs

Ask a Question

What is the pressure of the SF6 gas in the HVL/cc switch epoxy bottle?<br />

For 5kV and 15kV the gas pressure is 0.4 bars or 5.8 PSI. For 25kV and 38kV the gas pressure is 22 PSI

CTA-ID : 2032339
Was this helpful?
What can we do to improve the information ?