Technical FAQs

Ask a Question

Can a generator kit be obtained for older load centers like a QOC20MW225, Series L7?

Issue:
Product availability

Product Line:
QO Load centers

Environment:
Generator kit accessory

Cause:
Application

Resolution:
No, but the QOC20MW225 is ONLY a cover number. The old load centers that used this cover type, was not designed for use with Generator kits. A current design load center would need to be obtained for the generator kit accessory.




CTA-ID : 2032112
Was this helpful?
What can we do to improve the information ?