Technical FAQs

Ask a Question

What boot is available for use with the multi-speed pushbutton operators typically used in 9001 SKYP pendant stations?

9001 KU37 is a single boot which can be used with the 9001 SKRU2 through 5 pushbutton operators. Since the 9001 SKRU buttons come in pairs, two boots are needed per pair of pushbuttons.


CTA-ID : 2031950
Was this helpful?
What can we do to improve the information ?