Technical FAQs

Ask a Question

What is the pollution degree rating on the Altivar ATV66?

Pollution Degree 3 Per Nema ICS-1 and IEC 664-1


CTA-ID : 7004
Was this helpful?
What can we do to improve the information ?