Technical FAQs

Ask a Question

When mounting a MGA36800 in the I-Line panel are the screws that secure the breaker in place to engage a hole or a slot?<br />

With the MGA breaker the screws will actually engage with a slot not the hole.

CTA-ID : 2032067
Was this helpful?
What can we do to improve the information ?