Technical FAQs

Ask a Question

What is the part number for a fuse clip on a H366N, series E4?

Individual fuse clips are not replaceable. Customer will need to order a complete Line or Load Base.
Line base assembly - 40552-185-50 SEL (3-required and arc suppressor assembly is not included)
Load base assembly - 40552-187-50 SEL (3-required)



CTA-ID : 2031994
Was this helpful?
What can we do to improve the information ?