Technical FAQs

Ask a Question

Customer needs the white side bearings for an 8502/8536SFO1 NEMA Size 4 ?<br /><br />

Customer should order part number 3109102552 which is the housing, bell crank, side bearings and center bell crank bearing.


CTA-ID : 2031599
Was this helpful?
What can we do to improve the information ?