Technical FAQs

Ask a Question

What form is used to order 50 degree C calibrated circuit breaker FA34100

Use the suffix -35, These breaker are not UL listed


CTA-ID : 2031560
Was this helpful?
What can we do to improve the information ?