Technical FAQs

Ask a Question

What is the diameter / thread size of the 9049EF1 rod ?

It is 1/8`` diameter; 1/8 x 27 thread


CTA-ID : 2032216
Was this helpful?
What can we do to improve the information ?