Technical FAQs

Ask a Question

Is a LA400S UL listed as suitable for use as service equipment?

Yes, when the appropriate circuit breaker is installed - and appropriate solid neutral and service ground kit.


CTA-ID : 2031571
Was this helpful?
What can we do to improve the information ?