Technical FAQs

Ask a Question

What is the replacement solid state overload relay for use with an 8536 SG Nema Size 5 Starter which has an existing melting alloy overload relay using ``DD`` thermal units or a bimetallic overload relay using ``AF`` thermal units when the existing overload relay does not have a current transformer or is not CT (current transformer) driven?

Issue:     
Identifying part number for replacement overload relay for NEMA size 5 starter 

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Replacement SSOLR needed

Resolution:
Overload relay assembly that includes the current transformer:
Class 10 - 9065 SS5109 (45 - 135 A); 9065 SS510 (90 - 270 A).
Class 20 - 9065 SS5209 (45 - 135 A); 9065 SS520 (90 - 270 A).
Class 10/20 - 9065 SF5209 (45 - 135 A); 9065 SF520 (90 - 270 A).


CTA-ID : 2031930
Was this helpful?
What can we do to improve the information ?