Technical FAQs

Ask a Question

What are the torque specs on a PK15GTA?

The Torque Specs for a PK15GTA are: #14-10 cu or #12-10 al - 20 lb-in, #8 cu/al - 25 lb-in, #6-4 cu/al - 35 lb-in, and 2 wires #14-10 cu or 2 wire #12-10al 25 lb-in.


CTA-ID : 2031438
Was this helpful?
What can we do to improve the information ?