Technical FAQs

Ask a Question

What are the differences between the RU3040D400CL and RU3040D400FL Combination Service Entrance Device All-in-Ones?

Issue:
Product Features

Product Line:
CSED

Cause:
Product feature design differences

Resolution:
The RU3040D400CL is a surface mount device, convertible to semi-flush with a field installed FK400 flange kit (ordered separately). The RU3040D400FL is electrically equivalent, but is a semi-flush mount device only, with the semi-flush top endwall factory installed and sidewall flanges factory included.


CTA-ID : 2031651
Was this helpful?
What can we do to improve the information ?