Technical FAQs

Ask a Question

What is the replacement tenant main for a MP642R.

Requires the use of UL Type: Q2 tenant circuit breakers.
Original tenant breakers for this device were; Q2M2200, Q2M2200VH, or Q2MH2200.
Available in ampere ratings from 100A to 200.
New tenant circuit breakers for use in this device now include; QBP22200TM, QDP22200TM, or QGP22200TM (42 kA SCCR Max.).
Available in ampere ratings from 100A to 200


CTA-ID : 2031613
Was this helpful?
What can we do to improve the information ?