Technical FAQs

Ask a Question

Can the Altivar ATV66 drive run a Synchronous motor?

This can be done with a Synchronous reluctance motor. If the motor requires separate field excitation then this cannot not be done.


CTA-ID : 7030
Was this helpful?
What can we do to improve the information ?