Technical FAQs

Ask a Question

Is the handle of a 82355R double throw safety switch lockable from the outside in the center, down, and up position?

Yes. This unit handle is factory drilled with holes in the handle plate that make it lockable in the up, down or center position. The use of a customer supplied external padlock is required. No special SPLO suffix for factory drilled holes is needed.

CTA-ID : 2031901
Was this helpful?
What can we do to improve the information ?