Technical FAQs

Ask a Question

What is the difference between a KAL936150WB AND KAL36150WB ?

The `` 9 `` indicates a breaker that is UL Listed for Marine Applications on vessels over 65` in length . The breaker has no aluminum or aluminum alloy composition and is calibrated for an ambient of 40C .


CTA-ID : 2031757
Was this helpful?
What can we do to improve the information ?