Technical FAQs

Ask a Question

What is the replacement for busway ST13 and can they use their existing plug in units with the replacement busway?

ST13 Busway was replaced with the AP13 Busway and the plug in units were compatible. However, now the AP13 has been replaced by the new 100 amp Powerbus - PBCP3A100ST120 shown in Digest 173 on page 10-2. The plug-in units from the new Powerbus are not compatible with the older ST13 busway nor the older AP13 busway.


CTA-ID : 2031643
Was this helpful?
What can we do to improve the information ?