Technical FAQs

Ask a Question

Are the QO-GFI breakers Switch Duty Rated?

Issue:  
I need to know if my QO ground fault breakers are switch duty rated (SWD).  

Product line:  
Residential load centers

Environment:  
QO Circuit Breakers 

Resolution:  
No, they are not UL listed as switching duty rated (SWD).  
Was this helpful?
What can we do to improve the information ?