Technical FAQs

Ask a Question

Does Square D offer Heavy Duty Safety Switches in a Type 316 stainless steel enclosure?

Issue:
Product Availability

Product Line:
Heavy Duty Safety Switches

Environment:
Enclosure material

Cause:
Application

Resolution:
Yes, a limited number of Heavy Duty Safety Switches, 30A - 600A, are available in Type 316 stainless steel enclosures. They are limited to 3 Pole, 600V, fusible and non-fusible. The Type 316 devices will have a "SS" catalog number suffix.


 
Was this helpful?
What can we do to improve the information ?