Technical FAQs

Ask a Question

What is the AIC rating of a main breaker interior NQOD20M100CU? Can it be made to achieve 22K AIC?

The main breaker factory installed in that interior is catalog number QOB3100, so the panel AIC is 10K. To obtain a 22K panel, the main breaker must be changed to a QOB3100VH or the panel must be factory assembled as a 22K.


CTA-ID : 2031919
Was this helpful?
What can we do to improve the information ?