Technical FAQs

Ask a Question

Powerpact R frame unit mount: off end terminals move back and forth about 1/4 inch. Is this okay?

Yes. This terminal is not bolted down internally. It is just encapsulated in the moulding. It is allowed to move around because it has an internal connection that is flexible.


CTA-ID : 2031920
Was this helpful?
What can we do to improve the information ?